Hi I'm currently build the project
DRV830x-HC-C2-KIT_v105\PM_Sensorless to build F28069 platform
and I trying to mitigate the
HVMotorCtrl+PfcKit_v2.1\HVPM_Enhanced_Sensorless_2803x
which featuring eSMO and HFI
but I'm facing the problem following
"D:/ti/controlSUITE/libs/app_libs/motor_control/libs/HFI/v100/lib/HFI.lib" "D:/ti/controlSUITE/libs/app_libs/motor_control/libs/eSMO/v100/lib/esmo.lib"
error: file
"D:/ti/controlSUITE/libs/app_libs/motor_control/libs/eSMO/v100/lib/esmo.lib<
eSMO.obj>" specifies ISA revision "C2800", which is not compatible with ISA
revision "C28FPU32" specified in a previous file or on the command line
error: file
"D:/ti/controlSUITE/libs/math/FPUfastRTS/V100/lib/rts2800_fpu32_fast_supplem
ent.lib<sin_f32.obj>" specifies ISA revision "C28FPU32", which is not
compatible with ISA revision "C2700" specified in a previous file or on the
command line
what can I do for that..