According to the pinout info (SPRS902B), GPIO72 (pin 80) needs to be low, GPIO84 (pin 85) needs to be high, and TRST needs to be low (via a pulldown resistor). The boot sequence is reset, send in "A" to set baudrate, and then download a hex file to the SCI. In the PZP package, the default SCI IO pins are GPIO85 (pin86) and GPIO84 (pin 85). i.e. a clash.
Any idea how to deal with this?
Can anyone point me to a hardware solution?