C2000 Team,
The F2837xD datasheet, SPRS880G, Table 5-43 shows two specs for minimum ADC sampling window: 320 ns, and 1 ADCCLK.
In light of the first row in the table, the minimum ADCCLK is 5 MHz, which is 200 ns. Therefore, you cannot achieve 1 ADCCLK for the minimum sampling window since that would violate the 320 ns spec. It seems in reality the minimum sampling window is 2 ADCCLK in 16-bit mode.
There is somewhat misleading information as well in Table 10-29 of the TRM, SPRUHM8E, which states that the minimum acquisition time is one ADCCLK cycle, with no mention of the 320 ns (16-bit mode) minimum.
Can you advise?
- David