All,
I use the TMS320F28034PNT in the project of solar inverter,now our customer meets the issue as below:
1、The solar panel are obscured by the cloudy or others,the voltage of output is step-down slowly from 150V to 90V,the output of LDO reduce from 3.3V to 2.8V.
2、The MCU resets agine and agine because of the VDD less voltage,the reset chip is max308,the MCU will be locked after a certain number of reset.
3、Now I want to know the belwo issue:
1)How may reset times that the MCU will be locked?
2)How do we solve this problem of the MCU locked.