Hi All,
I have a project of solar inverter,TMS320F28335PGFA is used in the production,now our engineer measure the surface temperature
of MCU closes to 85℃(the Operating Temperature Range is -45-85℃),this is the air temperature that the distance is 10mm from the surface of MCU.
Please help to check if the measuring method is right or not,if not,please avdvise your suggestion,thanks.