My program is to big to run from memory. So in both release and flash my code is runs form flash (and copied to memory in the code). Only my code works if I run it in release and doesn't in flash. I think it is a timing issue. because I noted that my code runs slower in Flash.
So any suggestions what can be the cause? Interrupt handling?? And how to debug this issue.
I"m using the 28069M with CCS 6.1.1. and compiler 6.4.11
Thanks!