Hello,
I recently purchased the Piccolo F28075 Experimenter kit. I installed the ControlSUITE and imported the blinky project to get things started.
Build goes fine but on trying to start debugging, I get the error saying
"IcePick_C_0: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.641.0) "
I am using the CONTROLCard in the debugging configuration (SW1 and A:SW1 configurations are given as per the document in the ControlSUITE).
I have no reason to assume that anything is wrong with my installation. The XDS100v2 device is detected by my Windows PC and the Test connection in CCS is able to run the diagnostics. Just that the results come out as failure.
The worst part is I have purchased 2 of the kits and the same error persists in both of them.
I noticed that the .gel file for the F28075 is missing. Its not there in the ControlSUITE files that are shared. Does it have to do with the error?
Please help!!
Thanks,
Mathew