Hello,
According to the datasheet, when using LIN module in SCI multi-buffer mode, the transmission is initiated once byte 0 is written (bit TD0 in LINTD0 register). I am doing some tests in loopback mode and the transmission is initiated once either byte 0 or byte 1 are written. Is there a workaround to fix this issue?
Also, I would like to know if in SCI multi-buffer mode the RXRDY flag is set when the buffer of the configured length is full or every time there is a new character in the buffer. From what I understand from the datasheet, the latter is the answer, but I would like to confirm this.
Thanks