Hello everyone!
I have a problem when running a gui application included in ControlSuite libraries, to be more accurate, this is a PVInverter_F2803x code. First things first..
I'm trying to use the incremental built no.2 aiming to use a bulb as a load and to do so, I followed these steps:
1. I used a connection scheme from the instruction as a refrence
2. I established a successful concetion via the JTAG interface
3. I set an appropriate built option
4. I used the right expressions with the q-values obtained from a main.c file
The point is that even though I change the light intensity, the only value to follow this change is the theoretical power of the panel.. The rest of the values remains equal to 0, regardless of any changes. And now I got a question for you:
Do you have any idea what went wrong? I have no clue what more can I do, since I followed the instructions step by step.. but maybe some of you have encountered a similar problem and managed to solve it.
Thank you for your answers!
Igor