Hi,
I wanted to use the CC3200MOD design files as a reference for a project, but I realized that the .brd and gerber fiels don't open in Eagle or KiCad. I noticed an allegro.jrl file in the folder, was the board designed with Cadence Allegro? If so, do I have to use Allegro to work on the board or is there a library I can export to Eagle? If I don't own Allegro, can I view and edit the file somehow in another CAD software?