Hi
I have build a PCB board with the TMS320F28377S delfino and until now everything worked very well without any problems.
in the last couple of days i have "played" with SPI communication protocol to MEMS sensor , and now i have a short circuit in my board ( i have measured 16ohm resistance between VDD and ground ) and it seems that the short circuit is inside the TMS320F28377S chip because as i connect voltage to the circuit he gets warm very fast (other components dosnt) .
i am pretty sure that somehow i didnt used/connect the SPI signals properly and i damaged some I/O internal circuit .
the sensor i/O voltage is also 3.3V so i didnt used any buffer .
be happy if some one can advise me , maybe adding serial resistance or buffer will be a good practice?
best regards
Mark