My customer test the 28377D USB recently , and they can connect the ordinary U flash drive , but when they connect an I-flash Drive, 28377D can't identify.
the I-flash Drive is as link in description.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My customer test the 28377D USB recently , and they can connect the ordinary U flash drive , but when they connect an I-flash Drive, 28377D can't identify.
the I-flash Drive is as link in description.
Shuai Peng said:You mean the DSP only supports NTFS format?
Rather the other way round. The USB driver is for FAT file system and not NTFS.
Shuai Peng said:In addition,I doubt that dose 28377D supports USB3.0.
No driver support as of now. Though USB 3.0 being backward compatible should work at USB 2.0 speeds.
Regards,
Gautam