I want to build tms320f240 project, but can't find the tms320f240 cpu on ccs5.5 , just have f28x dsp on c2000, what ccs version have this cpu ? can you give me the download address? thanks very much.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to build tms320f240 project, but can't find the tms320f240 cpu on ccs5.5 , just have f28x dsp on c2000, what ccs version have this cpu ? can you give me the download address? thanks very much.
Chao,
TI announced "End-of-Life (EOL) status for F240 devices 4 years back. This device is no more sold/supported. If this is a new project, I strongly urge you to migrate to the c28xx family of devices.
F240 support is not available in CCS5.x or CCS6.x. It is only available in CCS3.3 and before.
Chao,
As Hareesh said, the F240 devices were end-of-life'd several years ago. There really is no support for them anymore. I don't believe there ever was a C24x simulator in Code Composer Studio. I looked at my installation of CCSv3.3 and there is no C24x or C2xx simulator. Even if there was a simulator in an even older version of CCS, it would only have simulated the CPU core (no peripherals). You can do the same thing with actual hardware if you already have a board (e.g., doing sustaining engineering on some existing product). If you don't already have a board, you shouldn't be using F240. Again, this product is no longer available and there is no support for it.
Appendices B, C, and D of the C28x CPU User's Guide SPRU430F contains information on C24x to C28x migration and instruction differences. My personal opinion is that trying to run C24x assembly code on the C28x is not the way to migrate. I would just re-write the C24x code in C and run it on the C28x like that. If you have an ultra time critical function, maybe re-write just that one in assembly on the C28x.
Regards,
David