Hi,
I've developed a custom development board for F28335 DSC. Seems like the JTAG pin connections are correct, but it is unable to detect the target. Some things that are not correctly working are,
1. Neither the XRSn pin is toggling nor the XCLKOUT pin is not outputting anything.
2. The XRSn pin remains in HIGH and comes to LOW when RESET switch is pressed.
3. The device is not detecting at all.
From where can I start troubleshooting? What are the possible reasons for this?
Any help would be appreciated..
Thanks,
Vishnu