Hi Team,
Looking at figure 25-15 on p. 2447 of the TRM for the TMS320F2837xD, I have the following question:
On the FLASH memory the Address bus uses the Delfino’s Addr[12:1] and then they show Addr[18:13] driven by GPIOs on the TI DSP.
Since the DQM0 to DQM3 (byte enables) are multiplexed with the EM1_Addr[15:18], my question is can I still use the EM1_Addr[15:18] as address bits of the FLASH or do I have to specifically use GPIOs on the Delfino to the Flash memory to cover Addr[15:18]?
Thanks,
Steve