Hello,
I am a Chinese student ,with a long time learned about the 2 phases Interleaved PFC kit, I made my 3.5 kw ILPFC hardware based on it.My PFC board is alsodesigned to connect a F28035 control card without a board Emulator through DIMM100. So I made a extra board emulator XDS100V1, which designed only withFT2232D and ISO724xs, use to connect my control card through 16 pin header(14 pins Jtag and 2 pins SCI) .
With the help of the ILPFC V1.1 code project , my pfc board works well at 110V/50Hz AC input at output power range 100~600w,and the PF is 0.99.Unfortunately,when I go on to add output power,the output voltage is down .The same situation happened when I add output power up to 800W under 230V/50Hz AC input.No more than that , the input current is not sin cave .
Therefor ,I want to adjust the control loop parameters . CCS could programm and run the target well until I change the Input AC voltage from 0 to 120V.I mean that while the Vbus is reaching 160V (PFC open voltage),CCS can't connect target anymore .The test data is upoload.
Now my problem is that
1. is there any one could guide me to improve my board emulator's anti-noise capacity?
2.without the Emulator ,could I adjust loop parameters using Compensator on main.cfg page?
3.To improve output power ratting and maintain the output voltage, which way should I think about?
4.to improve PF like below figure ,the outer Vloop or inner Cloop which one should I adjust?Could anyone tell me how to adjust?
Thank you!