This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with ePWM 11 in F28075 Experiment kit

Other Parts Discussed in Thread: CONTROLSUITE

Hi Guys,

CCS v 6.2(compiler version = TI v15.12.3.LTS)

TMX320F28075 Control Card

control Suite v 3.4.1

Example program used: ..\controlSUITE\device_support\F2807x\v200\F2807x_examples_Cpu1\epwm_up_aq

I modified the EPWM3 configuration to EPWM11 (replaced Epwm3Regs with Epwm11Regs).

I have enabled the clock for epwm11. I have initialized the epwm11 GPIO as:

void InitEPwm11Gpio(void)
{
    EALLOW;
    //
    // Disable internal pull-up for the selected output pins
    // for reduced power consumption
    // Pull-ups can be enabled or disabled by the user.
    // This will enable the pullups for the specified pins.
    // Comment out other unwanted lines.
    //
    GpioCtrlRegs.GPAPUD.bit.GPIO20 = 1;    // Disable pull-up on GPIO20 (EPWM11A)
    GpioCtrlRegs.GPAPUD.bit.GPIO21 = 1;    // Disable pull-up on GPIO21 (EPWM11B)

    //
    // Configure EPWM-11 pins using GPIO regs
    // This specifies which of the possible GPIO pins will be EPWM11 functional
    // pins.
    // Comment out other unwanted lines.
    //
    GpioCtrlRegs.GPAMUX2.bit.GPIO20 = 5;   // Configure GPIO20 as EPWM11A
    GpioCtrlRegs.GPAMUX2.bit.GPIO21 = 5;   // Configure GPIO21 as EPWM11B

    EDIS;
}

And the Counter and CMP values are working, as you can see below:

Now I do not get outputs at Pin 68 (GPIO20) and Pin 70 (GPIO21) in the experiment kit. But the other epwm 1 nad 2 gives pwm outputs as expected. Please let me know what am I doing wrong?