I have a problem uploading the code. The error says..
C28xx_CPU1: If erase/program (E/P) operation is being done on one core, the other core should not execute from shared-RAM (SR) as they are used for the E/P code. Also, CPU1 will be halted to determine SR ownership for the CPU which will run the Flash Plugin code, after which CPU1 will be set to run its application. User code execution from SR could commence after both flash banks are programmed.
I have learnt that it is due to CPU not being halted while uploading.
Can you guide me as to how to halt the CPUs for uploading. Can you also provide a link or document that has more information regarding this.