Hello.
I have two questions.
1.Is it correct to confirm the table 24-15,page 2302, in the technical reference manual when I use EMIF2?
2.Is it possible to access the address space described in the table 24-15,page 2302, in the technical reference manual when I use EMIF2?
About table 24-15,page 2302, in the technical reference manual, it seems to described Row Address as 13bit.
But TMS320F28375s has only 12 EM2A pins according to the device specific datasheet.
Would you give me any advises?
Regards,
uchida-k