Hello.
I have two questions.
1.Is following description in the datasheet typo?
a. In the table 60 at the page of 78, bit 31-3 is reserved field.
b. In the figure 59 at the page of 80, reset value of the register is x.
2.How long does latched value remain if the GPxDAT register is written when GPIO is input mode?
For example, How long does latched value remain when GPADAT-GPIO7 is written 0 if GPIO is configured as input and pullup?
Regards,
uchida-k