Other Parts Discussed in Thread: DRV8301-69M-KIT, DRV8301,
Hi.
I'm currently designing my own motor controller for the TMS320F28027F and DRV8301. I've been experimenting with the DRV8301-69M-KIT, which has a ControlCard with the much larger F28069M MCU.
The problem that arises from this is that the Trip Zone (TZ) pins are shared with the SPI and SCI peripheral pins on the F28027F. While the F28069M has them separate so it can connect to the DRV8301 with SPI and still connect it's OCTW and FAULT lines to it's TZ pins. I assume after looking at the SPRS523K.pdf that the TZ pins are used to give the ePWM module direct hardware pin interrupt for fault conditions coming from outside so it can disable the PWM outputs.
So the question is, the faults can also be read by SPI from the DRV8301 registers, so should I rather poll it via SPI and see if any faults are present and then software disable the PWM outputs on the F28027F? As I need both the SPI and SCI peripherals on the chip, with SPI going to the DRV8301 so I can configure it, while the SCI is needed for hardware MCU-MCU communication.