Other Parts Discussed in Thread: DAC7574, CONTROLSUITE
Tool/software: Code Composer Studio
Hi all,
I am trying to test the I2C module of TMS320F28075, I am using the sample code of control suit which is written to eeprom v180. I have not connected any eeprom but i have connected both SDA and SCL to Vcc- 5V via a resister 3KΩ. Like this in the image.
But when i go to debug session, I see a start condition happening and Data is being sent (address only), 8 bit mode is being used, thereafter 8 bits(address) are generated but no stop condition is happening. BTW if address bytes sent is 0x98(10011000) the SDA refelects with (00110000) ie,
if 10101010(0xAA) is sent i am seeing 01010100 means left shifted data is being sent on SDA.
I have loaded the snap for reference too.
Channel 1 : SDA
Channel 2 : SCL
I have initiated I2C like this
I2caRegs.I2CSAR.all = 0x0098;
I2caRegs.I2CPSC.all = 6;
I2caRegs.I2CCLKL = 10;
I2caRegs.I2CCLKH = 5; 49k
I2caRegs.I2CIER.all = 0x24;
I2caRegs.I2CMDR.all = 0x0020;
I2caRegs.I2CFFTX.all = 0x6000;
Write operation
if (I2caRegs.I2CMDR.bit.STP != 1){
I2caRegs.I2CSAR.all = 0x98;
if (I2caRegs.I2CSTR.bit.BB == 1)
{
return I2C_BUS_BUSY_ERROR;
}
I2caRegs.I2CCNT = 1;
I2caRegs.I2CDXR.all = 0xAA;
I2caRegs.I2CMDR.all =0x6E20;
}
Can any one tell me what might be missing or issue is?
Thanks in Advance
LT