Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: TI C/C++ Compiler
Hello there,
we´re running a "LaunchXL-F28377S" Evalboard.
We´re facing the effect, that the application doesn´t start, if a too big array is defined, for example a double Array with 200 entries.
I don´t think it´s a lag of RAM, because the Compile doesn´t complain that, plus all the RAM is defined to be used for variables.
The effect is, that the application can be loaded to to flash with the debugger emulator and the visiual program pointer starts at the very first line
of main()
Once the run button is pressed, the application crashes.
Does someone have an idea?
best regards!!