Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
Here is the full error message:
Error connecting to the target: (Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may be one or more of: no XDS100 is plugged in, invalid XDS100 serial number, blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the XDS100 can be located.
CCS Version: 7.1.0.00016
ControlSuite Version: 3.4.6
Device Manager:
Programs and Features (Arranged by Publisher):
There are no FTDI drivers located in Programs and Features.
I have tried reinstalling CCS and controlSUITE a handful of times with no luck and the same error. I have tried multiple USB cables and the F2837xD controlCARD (which I am using) has worked before and nothing has happened to it. At one point, I had been trying to figure out a different issue and probably messed up the drivers then, but I don't remember everything I did. I am running Windows 7 64 bit. I have tried to use windows update to update the XDS100 drivers under the Texas Instrument Debug Probes and it does not find anything. I have run the xds100serial command-line utility and it returns:
No XDS100 emulators were found on the system.
The controlCARD is plugged in and receiving power.