Hello,
I have clamping diodes to protect the analog inputs (ADC), but I cannot find exactly how much voltage/current they will take.
I know that they "shouldn't" have more than VDDA and less than GND, but my clamping diodes will allow a little more than than (400mV). I added a resistor in series (215) so the current would be limited to something like +/-2mA.
The only spec I find in the datasheet is in the Absolute Maximum Ratings, note (3) Continuous clamp current per pin is ± 2mA.
If that limit applies to the analog inputs, I would be right at the limit, but that's a worst case that assumes that the internal clamping of the ADC has no voltage drop. In reality I may be much better than that.
I need a reliable design so I want to be sure I'm understanding the real limit.
Could somebody tell me a little more about the internal circuits and how much these inputs can take?
Thanks,
Max
The part number is: TMS320F28069