I would use 28377S to interface external 16-bit ASRAM up to 2Mx16. I tried to use Pin-Mux Tool and reading the technical reference manual, but I have the doubt about addressing space of ASRAM and if DQM byte enable is needed or not.
Using PinMux for 28377S package 176 PTP, if I enable DQM pins the maximum address bit is "A14" because "A15-A16-A17-A18" are blocked by "DQM[3-0]" pins.
This is a problem for me because I would reuse the same architecture of another project with F28335 with external 16-bit ASRAM that allow me to address up to "A18" bit address.
Please, can you clarify it and if I can use 28377S to manage up to 2Mx16 of ASRAM addressing space? How to configure pin Mux to have these resources?