Hi there,
I am using TMS320F28377D to control/drive a custom made dc dc converter. As now I have to try to control 2x converters, I wanted to ask you if it is possible to control one converter from CPU1 and the second one from CPU2 independently.
This is because my converter switching frequency is 200kHz and also my controls/PWM update etc run at 200kHz (I use one adc interrupt, occurring at every 5us, i.e. 200kHz), and I think that if I try to drive/control two converters from the same CPU at this frequency, the interrupt code will take much longer than 5us (200kHz) to execute, hence I wanted to drive one converter from CPU1 and another one from CPU2, if possible.
If you have any opinion/advice on this it would be great,
Thank you so much,
Leo