Hi,
Two questions about F28027 HRPWM:
1) What's the limitation of CPMA in up-down mode? 3~PRD-3?
2) Is there any way to achieve 100% duty cycle in HRPWM mode?
Br, Jordan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Two questions about F28027 HRPWM:
1) What's the limitation of CPMA in up-down mode? 3~PRD-3?
2) Is there any way to achieve 100% duty cycle in HRPWM mode?
Br, Jordan
Jordan,
In high resolution mode there is limitation on when HR is active w.r.t. the PWM period.
Below is the note from user guide:
In up-down count mode: when counting up, 3 cycles after CTR = 0 until 3 cycles before CTR =PRD,
and when counting down, 3 cycles after CTR = PRD until 3 cycles before CTR = 0.
-Bharathi.