I have an external device attached via an 8-bit wide bus on EMIF1. I want to use the DMA to talk to this device via the memory-mapped EMIF address space. The DMA only makes 16-bit accesses.
If I make 16-bit accesses via the EMIF address space will the access be divided into two 8-bit accesses? Where in the F28377D documentation is this stated?
My external device is 16-bit internally and requires that the 8-bit accesses via the bus are performed in a particular order (low address first). Is there a guaranteed order for the accesses made by the F28377D? Where in the F28377D documentation is this stated?