Tool/software: Code Composer Studio
I cannot connect to the target machine because of this error.
Error connecting to the target:
(Error -1155 @ 0x0)
Device may be operating in low-power mode. The debugger has forced the device to wake up. Choose 'OK' to attempt to complete the debug connection.
(Emulation package 6.0.407.3)
If I click OK - I am re-prompted with the same error - it is as though it can't take it out of low power mode.
Scenario - We were testing interruption of "in the field updates" (where host CPU updates Piccolo). The code was interrupted during FLASH programming with a power loss. The update was about 10% through the FLASH'ing process when power was interrupted.
I am normally able to recover from such failure by connecting the emulator and re-flashing the target. I have done so many times.
My co-worker has the same CCS/Emulator setup and gets the same error when attempting to connect to this same target.
We are using CCS 6.1.1.00022 with Blackhawk XDS560v2-USB Sytem Trace Emulator.
It seems now I have a bricked device that I can't recover.