Tool/software: Code Composer Studio
Hi,
I have a code that uses the ethernet uip example. It works perfectly in RAM but when I pass to Flash, it doesn't work more. It stops in this function:
// Wait for the previous transmission to be complete.
while(HWREGBITW(&g_ulFlags, FLAG_RXPKTPEND) == 1)
{
}
This part is inside the EthernePaketGetDMA function. I saw in the WireShark but any package is received anymore.
But there is a time that I started the code and it continously send:
00:00:00_00:00:00 00:00:00_00:00:00 0x0000 60 Ethernet II
Can anyone help me?
thank you