Hello,
I have a custom board with the F28M36P63C2 and an external crystal of 20MHz. If I run the blinky example (start by the V2 emulator) then the blinking frequency is about 600 kHz. Running the same software without emulator (standalone), then the blinking is only about 60kHz. So the execution speed seems 10 times slower.
Can it be something with the clock detection? Measuring the crystal shows that it has a stable 20 MHz. Does it probably take to long to start the crystal in standalone mode? We have the slow speed on 3 boards out of 20. The rest run fine...
Any hints are welcome.
Thank you very much,
Karlheinz