Part Number: TMDSSOLARPEXPKIT
Hello everyone.
I have a Solar Explorer Kit board, TMDSSOLARPEXPKIT. I am trying to run the demo PVInverter. On build 1, project build well, program loaded well, and it could run at first. However when I write "1" to ClearInvTrip, it stopped working and gave me this:
In Build 2, when I gave Gui_Invstart 1, it stopped working and gave me something the same like build 1 shown above. I think it has something to do with the inverter hardware, because everything was working well until inverter stepped in, then it all went wrong. How can I resolve this? If this is a hardware problem? I managed to run those two demo successfully before...
Best regards,
Yue