Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
I am working on a Piccolo F28035 Controller using CCS 7.
My controller is not working as a standalone system. I am using a docking station for programming and checking the outputs of its PWM pins.
Its running only in debug mode as soon the power is switched off, the program stops loading from the flash.
It is also showing me a warning
"creating output section "ramfuncs" without a SECTIONS specification "
I took some other code which is booting from the flash from my colleague, but when I am flashing the same code from my system, it is not happening.
The only difference is that I am using CCS7 while he is using CCS 6.
I have added Memcopy() function, initialized the flash InitFlash().
But still this issue is not resolved, even the other code which I took from my colleague, which is flashing correctly from his PC using CCS 6 is showing the same behaviour in my PC i.e. not booting from flash.
Please respond or give some support in this regard