Other Parts Discussed in Thread: SYSBIOS, TMS320F28379D
Tool/software: TI-RTOS
hi
I using TMS320F28377D IC.
I want make timer ISR.
but I can't make 30us(micro) TIMER in SYS/BIOS.
var Timer = xdc.useModule('ti.sysbios.family.c28.Timer'); var timerParams = new Timer.Params(); timerParams.startMode = Timer.StartMode_AUTO; timerParams.runMode = Timer.RunMode_CONTINUOUS; timerParams.period = XXXX; timerParams.periodType = xdc.module("ti.sysbios.interfaces.ITimer").PeriodType_COUNTS; var myTimer = Timer.create(0, '&myTickFxn', timerParams); |
the result of an experiment
period 10000 -> 4ms
5000 -> 2ms
500 -> 200us
100 ->100us
50 -> 100us
I can't not understand.
I using 200MHZ IC.
i think "1Count = 5ns"
Is there a limit?
How to make 30us priod timer interupt using sys/bios??
Already make no-os system.
It works well. 30us