Hi,
In my Concerto-based design I plan to use an external reference so I'm looking for some additional information on VREFHI input of the A/D converter peripheral, namely, the spurious characteristics of external reference input. It's my understanding that for every conversion there will be a batch of 13 current spikes on that pin - one for Start of Conversion event followed by 12 spikes during conversion itself (one current spike per bit). So here are my questions.
1. Are spikes in question follow with the ADC CLK frequency?
2. What is the magnitude and duration of these current spikes, worst case?
3. What's a max and min values of the switched weighted capacitors in the array used in that ADC?
4. What's a value of the on-resistance for analog switches used to switch weighted capacitors in the array?
5. What's a max settling time for voltages on weighted capacitors in the array during A/D conversion?
5. What's a max total value (including parasitics) of the VREFHI input capacitance that is seen by reference pin driver?
6. What are the static load requirements for the reference pin driver? The datasheet seems to provide the typical value of 100uA only but is totally mum on the possible maximum.
7. Is there any basic schematic detailing connectivity of the capacitive array to the reference pin that would help in simulating reference input circuit performance?
Please clarify these things for me.
Regards, Michael