Tool/software: Code Composer Studio
In a project that I am writing there is a program running in one sector of Flash and RAM which writes data to other Flash sectors using the Flash API in ROM. When this program is using the Flash API to write/erase Flash would you recommend having JTAG disconnected?
In the past two or three weeks I have experienced some strange behavior when this program writes/erases Flash with JTAG connected (and often with the CCS Expressions view on Continuous Refresh). This has caused two microprocessors to act abnormally and appear as though Flash and the Flash registers are completely unavailable via JTAG. Also the program on the microcontroller is no longer able to write/erase the other sectors of Flash on these two devices. When it runs without JTAG I have never seen this problem. Thank you for your help with this issue.