Other Parts Discussed in Thread: CONTROLSUITE
Tool/software: Code Composer Studio
I have made the sd_card_m3 example using FatFs vn0.04b work properly on my controlCard-based hardware (although the SD card is running on SSI2 instead of SSI0) and the SD functions in that code ll work properly; I can debug this project and the UI signals on UART0 continue to work properly.
I also have a separate CPS_DSTR_m3 project that works with a sister project for the C28 core, this pair have shared memory defined where the C28 writes values to the S0-S7 RAM and the m3 reads it. I tired to add the SD card functionality from the sd_card_m3 example project to the CPS_DSTR_m3 project but it doesn't work - crashes when I try to run function "ls". I tried to debug this project but the UI over UART0 stops working when I debug.
There's something odd going on that may be similar to the issue described by Grant E Pitel in this post Grant E Pitel says "The interrupt handler for uartstudio is conflicting with something (probably the SSI), which was causing code to enter a FaultISR. I worked around the problem by disabling everything related to UART debugging."
How do I disable "everything related to UART debugging" so that I can see if my issue is the same as he suggested?
I'm really stuck here because my code doesn't work and I can't debug it to find out why.