Other Parts Discussed in Thread: TMS320F28335,
Hello fellows,
I am developing a UPS hardware using F28335 microcontroller. For driving some relays, I am using GPIOs 30, 31, 84, 85, 86 and for initialization, I need to keep the voltage on these pins low to avoiding accidents.
However, even if I use a pulldown resistor of 1k Ohms on each gpio, (which is the minimum recommended in section 3.4.1 of www.ti.com/.../spraas1c.pdf) some pins remain high (GPIOs 84, 85, 86), with a voltage of about 1.5V, while the others (GPIOs 30, 31) go low with 0.12V.
How to pulldown GPIOs on TMDSCNCD28335 / TMS320F28335? Will it damage the GPIO if I use resistance lower than 1k Ohms?
Thanks for any support.