Other Parts Discussed in Thread: TMDSECATCNCD379D, TLK110
Tool/software: Code Composer Studio
Hi , everyone.
1\ I want to design EtherCAT ET1100 circuit using 28379D, describe the detail as follows: 8bit async datawidth
EM1CS choose CS2 or cs3 or cs4;
em1oe ->rd
em1we->wr
em1wait->busy set em1wait to 0;
GPIO84->ET_IRQ;
GPIO87->EEPROM_LOAD;
EM1BA0,EM1BA1;EM1A[13:0];
ED[[7:0];
GPIO88->SYNC0;
GPIO89->SYNC1;
how to set EMxDQM pins?
And above pins is proper to set?
2\ how to use SSC 5.11 to generate slave stack code ?
There are five options to choose ti chip. AM335x may be fit for arm, it is not proper.
The other options are all about TMDSECATCNCD379D.
So if I use my circuit design by myself ,how to choose and how to generate slave stack code?
3\ My circuit do not design C28X pin connect to EtherCAT RESET. Of course , EtherCAT RESET is connected to the C28x reset pin. Is it ok?