Other Parts Discussed in Thread: TMS320F28335, C2000WARE
We have an application that has been built to be executed in RAM for TMS320F28377S. Setting the boot mode GPIOs properly, we want to upload the application via serial interface and then immediately execute it, for example using the Texas Instruments C2000 Serial Flash Programmer application running on Windows 7.
We have met the following issues:
- The upload process is very slow: we have tried to change the ‘-b’ option, but the application does not start
- The last sent character the application always returns an error (for example, 00=0F)
I have the following questions:
- In order to fix the former issues, Texas Instruments C2000 Serial Flash Programmer application should be recompiled?
- Does another programming toll exist?
- With a TMS320F28335, we have experienced the direct upload sending the firmware file using a terminal application: it is possible to do the same thing with TMS320F28377S?