Other Parts Discussed in Thread: C2000WARE
Hi all,
Using one of the lab examples provided in the multi-day
workshop that took place few months ago I was able to
display the provided sinusoidal data on a single ADC
channel (connected to pin 30 which is labeled as AA0
on the back of the F28379D board). I gather the other A/D
channels appear to be, for example, on pin 29 (labeled
AA2 on back of the board) as well as the other pins
labeled AA__, ABx and ACx --..., there are 16 pins in total.
I'd like to know if you could point me to some example code
(or perhaps a modified version of one of those workshop examples)
that would work in such a way to acquire data on say 4 of these
channels concurrently. Would such concurrency in data acquisition
via multiple channels be possible on TMS320F28379D?
If so, would love to see an example showing such concurrency
as well as clearly identifying those involved channels.
Perhaps could be tried out as a separate project on the code
composer studio (v8). Many thanks.
- Saleh