Hi, I have a noise problem with the interface between the launchxl tms320f28377s and an FPGA, the development tool altera DE2. I connect the output of an EPWM module to initiate a state machine when the outputs are set to zero (Figure 1). In the attached figures, the outputs of the EPWM are the signals green and blue and the output of the FPGA is pink. Sometimes the state machine doesn't run I think that is due noise (Figure 2). I connect directly from the output of the DSP to the FPGA by wires, without any other component. How can I solve this problem? thanks.
Figure 1.
Figure 2