I am trying to run the PMSM Sensorless example code for the high voltage kit. I am using the EZ DSP for 28335 and the DRV8312 EVM eval module. I have a good 3.3V quadrature encoder signal to the EZ DSP on GPIO20, 21, 23 (A,B,I respectively). I am on incremental buil Level 3. When spinning the motor, I get a value of speed1.Speed=0. When I view the rg1.out I get a sawtooth. When I view qep1.ElecTheta, I get square pulses between 0 and 1. They are amuch higher frequency than the sawtooth of rg1.Out.
How should I go about troubleshooting this?
Thanks,
Brad Mularcik