Hello TI Officers,
I am using the LAUNCHXL-F28379D, and I have some questions:
1. I had an experiment where I connect 2 wires: GND and a voltage 3V to the board. But the strange thing is that, when I didn't even power the board, I connected my GND wire to the GND pin, and the 3V pin to any header pin except 3V3 or 5V (either GPIO pins or ADC/DAC pins), I saw the LEDs D9 lights up. Actually, I measured the TP13 and all devices connected to 3V3 line and 5V line are all having 1.8V. Why is that ? I can't believe that by supplying any GPIOs with a voltage the board would have voltage on the power supply line itself. That's not true isn't it ?
2. For this board, do I need to add any capacitance to the ADC pins to help the ADC process ?
Regards,
An.