Hi Everyone,
I am working on digital control 3 phase PFC, the converter use standard 6 switches inverter structure, implemented with Si MOSFET with Fsw = 50kHz, and I use Launchpad F28027 for my controller prototype.
I need to have continuous communication between my PC and the MCU to monitor some operating parameter of the PFC. I use the serial communication (UART) and internal FTDI IC as serial to USB.
My question is, now I use the circuit as inverter to test the basic function and feedback circuit when the input voltage increase above 170V, the communication link always broken. -
->>The inverter was tested and can work properly with input voltage up to 400V
Can anybody suggest me what should I do to improve the communication link?and what is the kind of EMI noise that cause it to fail?dV/dt noise?
- so far I tried to cover the MCU with faraday cage, but still fail
Thanks