Hello,
I am using the CARD Concert F28M36x control in simulink, but I have problems with the sample time, I do not understand how it works.
I am developing a control for buck converter.
When I select a sample time of 1 / (100kHz) the control works, but when I increase the sample time to 1 / (1MHz) the microcontroller does not work.
my questions are:
Does the sampe time depend on the ADC?
F28M36x has an ADC of 2.88 MSPS, should I be able to select 1 / (2.88 MHz) as the maximum sampling time?