Other Parts Discussed in Thread: CC2650
Tool/software: TI-RTOS
To burn the SampleSwitch project on the cc2630 launchPad, the sleep power consumption is about 8 uA. However, the DCDC _ SW and VDDR are grounded, and 1.8 V power supply is used, only the configuration in cfg. c is modified, and the sleep power consumption is about 130 uA. the configuration of the cfg. c modification is as follows:
#define SET_CCFG_MODE_CONF_1_ALT_DCDC_VMIN 0x0
#define SET_CCFG_MODE_CONF_DCDC_RECHARGE 0x1 // Do not use the DC/DC during recharge in powerdown
#define SET_CCFG_MODE_CONF_DCDC_ACTIVE 0x1 // Do not use the DC/DC during active mod