Hi,
Customer is using F28235 Q100 for their application. 20MHz external crystal is used.
Here are some doubts:
1) Can 20MHz be used? It should be OK.
2) What's the recommendation for CL and other specifications?
Thanks a lot.
Br, Jordan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Customer is using F28235 Q100 for their application. 20MHz external crystal is used.
Here are some doubts:
1) Can 20MHz be used? It should be OK.
2) What's the recommendation for CL and other specifications?
Thanks a lot.
Br, Jordan
Jordan,
The max PLL multipler is 10/2. You will only be able to achieve 100 MHz operation with a 20 MHz crystal. You can use 20 MHz with that restriction.
Normally, people use 30 MHz crystal with F28235 to achieve 150 MHz operation.
Regards,
David
The parameters for the passive components vary based on the crystal chosen. Hence we do not recommend any values. Our datasheet has the following note:
TI recommends that customers have the resonator/crystal vendor characterize the operation of their device with the DSC chip. The resonator/crystal vendor has the equipment and expertise to tune the tank circuit. The vendor can also advise the customer regarding the proper tank component values that will produce proper start-up and stability over the entire operating range.