Hello,
I am trying to communicate between two LAUNCHXL-F28069M boards using SPI communication. One board is master and other is slave. I have successfully sent data from master to slave ( data is like this 11, 22, 33, 44 or any other integer or character). I have seen the received data on slave side and trying to re-transmit that data to the master. While re-transmitting I am facing problem that the data is received as 44, 11, 22, 33 instead of 11, 22, 33, 44. Why my last value is coming first in re-transmission. I have checked the whole code, but I did not get any significant reason behind this. Please tell me what could be the reason. I have simulated this in matlab (using simulink and embedded coder support package) . Is it something related to SPI protocol ?
Regard,
Nisha